המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why are the IP Address, Mask and/or Gateway not saved when using Ethernet IP on ATV630 drive after a power cycle?
Issue:
IP Address, Mask and/or Gateway are not saved when using Ethernet IP on ATV630 drive after a power cycle.

Cause:
The Mode "Fixed" was not selected when up the IP.

Resolution:

To avoid the loss of the values IP Address, Mask and/or Gateway when the device is power cycled the IP Mode must be set to "Fixed"
SETTINGSCODEVALUEDESCRIPTION
[FIXED]MAnU0Manually set the IP address.
[BOOTP]bOOt1Automatically gets the IP address from the Bootp or DHCP server using the Bootp or DHCP server using the MAC address.
[DHCP]dHCP2Automatically gets the IP address from the Bootp or DHCP server using the Factory setting: DHCP



If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)