המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How many simultaneous connections you can have with Vijeo Design'Air Plus?
Issue:
How many simultaneous connections you can have with Vijeo Design'Air Plus?

Product Line:
Vijeo Design'Air Plus, Vijeo Designer

Environment:
Remote access from Android/iOS phone/tablet to physical Human Machine Interface (HMI)

Resolution:
Vijeo Design'Air Plus from a single HMI only allows one connection at a time from a single phone or tablet.