המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Wrong data could be returned with I/O scanner on BMXNOE0100 when used in a large system and multiple NOE's are scanning each other.
Issue
Wrong data  could be returned with I/O scanner on BMXNOE0100 when used in a large system and multiple NOE's are scanning each other.

Product Line
BMXNOE0110

Environment
Unity, Control Expert

Resolution
This is corrected by upgrading the firmware to version 3.0 or greater