איך נוכל לעזור לך היום?

How to add DO and DA quickly in application setting of 140NOP85000

User need to set the initialization value of the DAs, so they will do it in application setting of IEDCT
Sometimes there are many DAs, so IEDCT support "Add ALL" of them. but some PC can't see the "ADD ALL" button because the button is at the bottom and cover by taskbar, please refer to the picture because of the PC display rate