המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
ATS01N222RT Can you do a soft stop?
Issue:
How do I get the ATS01 to soft stop?

Product Line:
ATS01 Altistart 01 Altivar

Environment:
ATS01.....RT

Cause:
Need soft stopping.

Resolve:
If you have a jumper between LI2 and LI+ terminals, you will have soft starting with line power and a coast to stop when line power is removed.

If you have a start-stop signal that closes LI2 to LI+ to start, it will soft start according to the start dial.  When you open this contact it will soft stop (decelerate) according to the stop dial setting.