המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Video: How add a link to an external file in the Vista application for viewing on web

Issue
Vista file linking is limited, and does not allow documents to be opened

Product Line

Struxureware Power Monitoring 7.0(SPM)

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Vista

Cause
By default you cannot link to files other than  .exe .bat and .CMD.

Resolution
The following method will allow you to link to an unsupported file extension.
This will enable you to access files such as user guides from the Vista application and the web.

Please note that documents will still need its corresponding application installed to open properly.
Example: If you need to view a  PDF file , the target machine will need Adobe reader installed to view the file properly.