המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the TTL for a Quantum 140NOC78x00?
Issue
What is the TTL (Time To Live) for a Quantum 140NOC78x00?


Product Line
140NOC78000
140NOC78100


Resolution
For a Quantum 140NOC78x00 with firmware versions less than 1.70, the TTL (Time To Live) for Point to Point EIP communications through routers, is 1.

For a Quantum 140NOC78x00 with firmware versions equal to or greater than 1.70, the TTL (Time To Live) for Point to Point EIP communications through routers, is 64.

The TTL remains at 1 for Multicast EIP communications.

If a TTL greater than 1 is required for Point to Point EIP communications, then upgrade the 140NOC78x00 firmware to version 1.70 or higher.