המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Error "HTTP Error 404.3" shows in the webpage while trying to run Reports in PSE

Issue

Customer getting "HTTP Error 404.3" when trying to run a Reports in PSE

Product Line
Powerlogic Scada 8.x (PSE 8.x)

Environment
Report creation, trying to pull historical data store in the PME system using the PSE interface

Cause
IIS (Internet Information Services) is not set up properly.

Resolution

Install IIS subcomponents from

  • Start-->Control Panel --> Programs and Features --> Turn Windows features ON or OFF.
    Programs and Features
  • In Internet Information Services--> World Wide Web Services -->Application Development Features
    Windows Features
  • Check ASP.NET (.NET Extensibility, ISAPI Extensions, ISAPI Filters will be selected automatically).
    ASP.NET check box
  • Double check that specific versions are checked
  • Open the Command prompt by clicking on start and select run and type in cmd-->enter, and type and run the following:
%windir%\Microsoft.NET\Framework64\v4.0.30319\aspnet_regiis.exe -ir


Successful command prompt entry

  • Finally check in IIS manager, that your application uses application pool with .NET framework version v4.0