המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do you set up an external input with an active low to trigger an external fault on an Altivar Process Drive?
Issue:
Can an external input with an active low to be programmed as an external fault on an Altivar Process Drive?

Product Line:
Altivar 930 and Altivar 630 drive

Environment:
All

Cause:
Wants to turn off a digital input and have the drive trigger an external fault.

Resolution:
Programming:
From Complete Settings and press enter
Go to Error/Warning handling and press enter
Select External Error and press enter
Ex error assign enter and choose DI1 thru DI6 Low  (you must scroll all the way down to the bottom of the selection menu.)
set the external fault as DI1 Low