המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
When do the cooling fans run on the ATV630 Process Drives?

Issue:
Cooling fans run adjustments on ATV630 and ATV930 Process Drives

Product Line:
Altivar ATV630 and ATV930

Environment:
All

Cause:
Wants to know when the fans run on the drive.

Resolution:
The fans for the drive up to 90kW can be run in 3 modes :

- Standard : at run order
- Always : the fans run permanently
- Economy : The fans run according to the drive thermal state

For the drives upper than 90kW, the fans run only at run order.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)