המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What type of 3G modem can my Com'X use?
Issue:
What type of 3G modem can Com'X gateways use?

Product Line:
Com’X 200/210/510

Environment:
Com’X 200/210/510 with 3G Modem communication

Resolution:
The following 3G modems have been tested and are compatible with the Com'X 200/210/510.
For each modem, refer to the manufacturer's documentation for technical specifications and detailed installation instructions.

Manufacturer/ModelAntennaNotes
MultiTech MTC-H5 External Recommended
Connect to the Com'X gateway internal USB port.
This modem must be mounted to the enclosure externally.
Huawei MS2131i-8 Internal 55°C maximum operating temperature
Modem connects to internal USB port and mounts inside the Com'X gateway front door.
MultiTech MTD-H5 Internal Connect to the Com'X gateway internal USB port.
Modem must be extended outside the Com'X gateway front door