המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What parameters can be added to the ATV630 MyMenu?

Issue:
Needs to add parameters to MyMenu on an ATV630.

Product line:
ATV630, ATV600, Altivar Process


Resolution:
The MyMenu can only add parameters listed under the Complete Settings menu.  Other parameters, such as Motor Thermal State (THR) under the Display menu, cannot be added to the MyMenu.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)