המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
ATV61 or ATV71 drive will not recognize the VW3A3320 card or faults when installed.
Issue:
ATV61 or ATV71 faults after installing the VW3A3320 card

Product Line:
ATV61 and ATV71 drives.

Environment:
All

Cause:
Outdated firmware

Resolution:
Most likely an old firmware version in the drive.
Per the VW3A3320 manual: The EtheNet/IP Card (catalog number VW3A3320) is used to connect an Altivar 61/71 drive to an Ethernet network using the Ethernet protocol.  This communication option card is fully supported with the version V5.7 and above of the Altivar 61 firmware and with the version 5.8 and above of Altivar 71 firmware.