המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Video: How can I restore my Vista template diagram to the default configuration?
Issue:
The default vista diagram for a meter type has been edited and must be to restored it to its default configuration.

Product Line:
ION Enterprise 6.0
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023


Environment:
Vista

Cause:
If an edit is made to the template diagram, such as linking it to a specific node, that change will reflect across all diagrams for devices of that type. For example if a voltage measurement on the template diagram is linked to a specific node it will now only pull the voltage measurement from that device no matter which device of that type is being viewed.

Resolution:
The steps to restore the template diagram to the default state are covered in the video below.