המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do I set a bit when we press the ACKAll button an Alarm Summary in Vijeo Designer Runtime?
Issue:
How do I set a bit when we press the ACKAll button an Alarm Summary in Vijeo Designer Runtime?

Product Line:
Vijeo Designer (all versions)

Resolution:
To set a bit when pressing the ACKAll button on an alarm summary requires you to draw an invisble switch over the existing ACKAll button.

The invisible switch should have the following operations defined:
1) Alarms & Events --> AckAll on your AlarmSummary
2) Bit -> Set on your BOOLEAN Variable.