המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
On the Process ATV600 and ATV900 series drives, can a relay output indicate if the drive is in remote or local mode?

Issue:
Needs remote indication of whether the drive is in remote or local mode.

Product Line:
ATV600 ATV900

Environment:
All models and serial numbers.

Cause:
Information unclear in current literature.

Resolution:
The ATV600 and ATV900 Process drives have an HMI button for Local/Remote mode selection.  Relay indication of the mode can be established by setting the relay assignment to [HMI Cmd]. The relay is activate when the VFD is in Local mode.
Note that this feature was added to ATV600 V1.6.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)