המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Where can I find basic programming information for ATV drive?
Issue:
Basic programming information for ATV Drive

Product Line:
ATV930

Environment:
All

Cause:
Basic programming.

Resolution:

Under drive menu:

tCC = 2/3 wire control
CG = Macro con fig
bFr  = Standard motor frequency 60 hz
nPr = Rated motor power= HP size of the motor
UnS = Rated motor voltage =  motor voltage
nCr = Rated motor current= motor amps
FrS = Rated motor Frequency= 60 hz
NS = Rated motor speed= motor r pms
fFr = Max Frequency= Hz
Itch = Motor Thermal Current= Amps
ACC = Ramp up time acceleration
DEC = Ramp down time deceleration
LP = Low speed setting
HP =High speed setting

Command Menu:
RFR = AI 1 for remote pot control
= AI 2 for analog input 4-20 mA control
= (See the ATV programming manual for other options)
CHCP = Not separate or Separate (depends on where start/stop and speed controls are coming from)
RC = Reference switching.

Refer to the programming manual for in depth explanation and menu structure.