המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do we decode the Date of Manufacture (DOM) on the Magelis series of HMIs?
Issue:
Where on the label of the Magelis HMI can we find information regarding the date in which the unit was produced?

Product Line:
Magelis series of HMI, XBTG, XBTGT, HMIGTO, HMISTO, HMISTU, HMIGTU, HMIGK

Resolution:
On the back of a Magelis HMI, there is a sticker/label with the Date of Manufacture (DOM) on it. The code is typically 4 digits like this: 1533. For this particular example, it decodes as Year:2015, Week 33.

Therefore in general terms the date code is: YYWW where YY is the last two digits of the year and WW is the week number in that particular year.