איך נוכל לעזור לך היום?

PlantStruxure PES: How to integrate Altivar61/71 on Modbus TCP/IP in PES.

Goals and Symptoms

This document is created to explain the minimum configuration that we should do/ configure in order to have working good integration with expected behavior between Altivar 61/71 on Modbus TCP/ IP with PES.

Facts and Changes

This document can be used in any PES version.

Causes and Fixes

The PES help documents does not help at all to explain this integration so the users who are quite new with the Altivar product and PES will have big difficulties to implement this integration.
With this document, it can help the user to do the integration.

Refer to the attached document for details on configuration of Altivar and PES in details.

שניידר אלקטריק ישראל

קבצים מצורפים
Integration ATV61_71 with PES.pdf [1.28 MB]