המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can you run the ATV61 and ATV71 Drive without the HMI on the face of the drive?
Issue:
Can you run the ATV61 and ATV71 Drive without the HMI?

Product Line:
Altivar ATV61 and ATV71 drive

Environment:
All

Cause:
Wants to take off the HMI and still run the drive.

Resolution:
You can run the ATV61 and ATV71 drive without the HMI on the face of the drive as long as the drive is not programmed to be controlled with the HMI like wheel is the knob is the speed control or the start stop buttons are active.