המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Explain the serial number and how to identify date of manufacture for Altivar Process Drives.
Issue:
Trying to break down the serial number from the Altivar Process drive

Product line:
ATV630, ATV650, ATV930, ATV950, Altivar Process

Environment:
All

Cause:
N/A

Resolution:
Sample serial number from ATV630 drive - 4004700HL530989002

4004700 - Product Code (may or may not be on label)
HL530 - Date code.
HL - Manufacturing plant (also could be 6W, 8B, 88, N2, JM or Y1)
5 - Year, 2015 (6 = 2016, 7 = 2017, etc)
30 - week
989002 - Internal manufacturing data

*** Note that the 1digit YEAR code was changed to 2digits in 2018.  So, a drive manufactured in year 2022 week 8 has a date code 2208.


“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)