המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How can I get 5% line impedance for the ATV630 Process Drives?

Article available in these languages: Spanish

Issue:
Customer is looking for equivalent to 5% line reactor on the Altivar Process drive.

Product line:
ATV630, ATV600, Altivar Process

Resolution:
The drive's standard internal DC choke plus a 3% line reactor.  Adding an external line reactor will yield a 5% line impedance equivalence.
Schneider Electric does not offer Line reactors for the Altivar Process Drives.  Please contact a manufacturer, such as MTE Corp, for selection.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)