איך נוכל לעזור לך היום?

How should errors be checked in the DATA_EXCH function block of the M580 when using CIP messaging?

Issue
How should errors be checked in the DATA_EXCH function block of the M580 when using CIP messaging?

Product Line
EcoStruxure Control Expert, Modicon M580

Environment
Control Expert v14.1, BMEP581020 v3.10


Resolution
Error handling in the DATA_EXCH block is a bit more complex than for the other communications block due to the functionality of the block.
Se the attached document for an explanation of how to handle errors.

שניידר אלקטריק ישראל

קבצים מצורפים
Error Checking.pdf [198.86 KB]