המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the minimum mounting space between the top and bottom of the ATV212H series drives?
Issue:
ATV212HD15N4 mounting info needed on spacing mounting vertically.

Product Line:
Altivar ATV212 drive

Resolution:
The ATV212 installation manual has the Drive mounting generalities.
In this case the min mounting clearance between the top and bottom of the drive is 2 inches top and 2 inches from the bottom.

The ATV212 Drives side to side mounting is also 2 inches if the top cover is still in place on the drive.  If you remove the top cove you can mount side by side no minimum distance.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)