המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is an Altivar ATV320 rated for variable or constant torque loads?

Article available in these languages: SL

Issue:
Is ATV320 rated for variable or constant torques?

Product Line:
Altivar 320, ATV320 Machine Drive

Resolution:
The ATV320 is designed for both variable torque and constant torque loads.

In the Motor Control menu (drC-), there is a parameter Motor Control Type (Ctt) selection for the application.  Among others, the basic selection is:
Std (Standard) for a linear V/F ratio which is typical for constant torque loads
uF9 (V/F Quad) for a curved V/F ratio which is typical for variable torque loads

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)