המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the system requirement for Unity Pro v12 ?
System requirements

System with Microsoft Windows 7 Professional 32/64bits
System: Pentium Processor 2.4 GHz or higher, recommended 3.0 GHz
RAM memory: 2GB minimum; recommended: 4GB
Hard disk: minimum available free space 8 GB, recommended 20 GB
Microsoft Internet Explorer 5.5 or higher
On Windows 7 64bits System, installation of Windows 7 Service Pack 1 (SP1) is mandatory in order to use Unity Pro V12

Windows 7 Professional 64bits ,is recommended for projects using DTMs


System with Microsoft Windows 10 32/64bits
System: Pentium Processor 2.4 GHz or higher, recommended 3.0 GHz
RAM memory: 2GB minimum; recommended: 4GB
Hard disk: minimum available free space 8 GB, recommended 20 GB
Windows 10 64bits is recommended for projects using DTMs (example : projects using Modicon M580 controller)

System with Microsoft Windows Server 2012 R2
Recommended version: Windows Server 2012 R2, standard version
Processor recommended: 3.20GHz
RAM memory recommended: 16.0 GB

Important notice
Unity Pro requires .NET 3.5 and .NET 4.5.2
Depending on the target Windows version and Windows configuration, .Net versions may be
- not installed
- installed but not enabled ( the related "windows feature"  is not set ON )
- installed and enabled

Unity Pro setup tries to automatically install and enable the required .Net  on the target Windows if necessary.

On Windows 10 and Windows Server 2012 R2, automatic or manual installation of .Net 3.5 requires an internet connection.
And service “Windows Update” must be started in order to install the .NET Framework 3.5.

If automatic installation of  .Net 3.5  fails, please read & follow  Microsoft technical notes on .NET 3.5 installation:

- Installing the .NET Framework 3.5 on Windows 8 or 8.1
http://msdn.microsoft.com/en-us/library/hh506443.aspx