איך נוכל לעזור לך היום?

What is the purpose of the terminals in the middle area of BMXFTB2820

Question:
What is the purpose of the terminals in the middle area of BMXFTB2820
This image is not available because: You don’t have the privileges to see it, or it has been removed from the system

Answer:
This area is for measuring purpose, all these terminals in this area are breakover with the every normal terminals 1-16 which have cables connected.