המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
ATV320 -The manual states that bLF (Brake Logic Fault) can be reset by a logic input, but appears this does not work?
Issue:
With the the ATV320, the manual states that  bLF (Brake Logic Fault) can be reset by a logic input, but appears this does not work?

Product Line:
ATV320

Environment:
Brake Logic Fault

Cause:
n/a

Resolution:
France response:  That is correct, on actual ATV320 version BLF can be reset by power cycle or product reset (RP or RPA).
It is not possible to reset this fault with automatic reset or standard reset fault RSF.
Evolution request is already registered on this point (PEP0324717R).  Today, it is planned to have this change on maintenance version of ATV320 for end of 2017. I do not have more precise date for this release.
In the meantime, a workaround for you would be to reset BLF by a logic input, you can use the RPA function. This function will manage a product reset via a logic input and will reset the BLF.