המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to Enable Protocol Settings in RemoteConnect (Modbus RTU, Modbus TCP Server/Client, DNP3 Peer to Peer, etc…)

When a new project is created in RemoteConnect, users are prompted to choose the project settings for the SCADAPack configuration. By default, only MODBUS RTU Server is selected.

RCImage

Once a configuration has been created, users may wish to configure the SCADAPack for other protocol options. Without the proper project settings enabled, the configuration fields in RemoteConnect will not be visible. For example, There are no configuration options for the Modbus Scanner if the Modbus TCP Client or Modbus RTU features are not enabled in the Project Settings.

To configure the project settings for a RemoteConnect project, ensure the SCADAPack x70 object is highlighted in the Network view and click on the menu button. Select Additional Options -> Project Settings. You can then enable the project configuration options you desire and click OK.

RCImage2