המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can the M258 inputs DM72F0 and DM72F1 be used as regular inputs?
Issue:
Can the M258 fast inputs on DM72F0 and DM72F1 be used as regular inputs?

Product Line:
Modicon M258, SoMachine, EcoStruxure Machine Expert v1.2

Environment:
Embedded Discrete Transistor Inputs for Modicon M258 PLC

Resolution:
The fast inputs on the M258 are configured as regular inputs. by default:
(EcoStruxure Machine Expert v1.2 depicted below)
DM72F0 and DM72F1 I/O Configuration

To add a High Speed Counter, Event Latch, Frequency Generator, Standard Encoder or PWM generator, click on the green (+) button to the right of the DM72F0 or DM72F1 node (or use Right-click and "Add Device")
Add Device with (+) button

Choose an Expert module

For example with a High Speed Counter:
The node you choose (HSCMain in this example) will appear under the DM72Fx node (A).
Click on the "HSC Main Configuration" tab (B) to configure the parameters of Counter/Event Latch/etc.
Choose a Counting Mode under the General Parameters folder (C):
HSC Main example configuration