המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Video: How to configure Event Notification Module

Issue
The user needs instruction on configuring Event Notification Module to work with Power Monitoring Expert (PME) or PowerSCADA Expert (PSE)

Product Line
Event Notification Module (ENM)
Power Monitoring Expert (PME)
PowerSCADA Expert (PSE)

Environment
ENM Configuration

Resolution
The video attached depicts the process of configuring ENM. The following topics will be covered:

1. Configure Event Sources
2. Set the Filters
3. Configure a recipient
4. Define the schedule and the subscription method
5. Resetting the services
6. Define the maintenance control tags

**As of PME 2020, ENM has been modified to be included within the PME web applications in the form of "Notifications". Please see the following information for more details Event Notification Module configuration