המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What driver to use in Vijeo Designer to communicate to Allen Bradley Drive over Ethernet/IP?
Issue:
What driver to use in Vijeo Designer to communicate to Allen Bradley Drive over Ethernet/IP?

Product Line:
EIP, Magelis

Resolution:
Due to Vijeo Designer Rockwell EIP driver are specific to a controller type.  It is not possible to use that driver.  To communicate to any third party devices (including a AB drive) over Ethernet/IP, it is recommended to use the Ethernet/IP Explicit driver under Generic Drivers.