המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the analog input resolution bit size on the ATV32 and ATV320 Drives using ATV logic?

Article available in these languages: Czech

Issue:
Analog input resolution bit size on the ATV32 and ATV320 Drives using ATV logic

Product Line:
ATV32 and ATV320 drives

Environment:
All

Cause:
Analog input bit size resolution.

Resolution:
All the analog signals are represented internally in ATV32/ATV320 ATVLogic as 13-bit  (0..8192) + 1 bit for sign.
Below some example of AIx type and correspondence with value read by ATVLogic:
If AIx is 0..20mA type :
-> "0" read by ATLogic will correspond to 0mA.
-> "4096" read by ATLogic will correspond to 10mA.
-> "8192" read by ATLogic will correspond to 20mA.

If AIx is 4mA..20mA type :
-> "0" read by ATLogic will correspond to 4mA.
-> "4096" read by ATLogic will correspond to 12mA.
->"8192" read by ATLogic will correspond to 20mA.

If AIx is 0V..10V type :
-> "0" read by ATLogic will correspond to 0V.
-> "4096" read by ATLogic will correspond to 5V
-> "8192" read by ATLogic will correspond to 10V.

If AIx is -10V..10V type :
-> " - 8192" read by ATLogic will correspond to -10V.
-> "0" read by ATLogic will correspond to 5V
-> "8192" read by ATLogic will correspond to 10V.