המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Unity Pro V12/13 Data animation error on refine of DFB
If on a refine of the instance DFB in on line mode, variables are not well animated in the DFB: err value
see screen below. The issue can come of the naming of the variables.

If the name of the instance of the DFB is included in the first part of the name of the variable, example
instance name of the DFB is "par" and the variable name is "paris", the variable will not be well animated.


To correct this problem you need to modify the name of the DFB or of the variable.
for example par_1 as name of the DFB solves the problem.


This problem will be corrected in next version of Unity Pro.