איך נוכל לעזור לך היום?

Why the standby CPU display “cannot transfer plc reserved ” when application transfer from primary to standby?


Once the application protection is set, uploading application from CPU will require a password, and the HSBY transfer will be disabled, the standby CPU display message “cannot transfer plc reserved ”