How to change the IP address on Altivar Process drives (ATV900 / ATV600)
You can modify the IP address of Altivar Process drives (ATV600 and ATV900) either via the local HMI or using commissioning software such as SoMove.
The following video demonstrates the procedure:
Key steps shown in the video
Connect to the drive (locally or via SoMove)
Navigate to the Ethernet / communication settings
Select the IP assignment mode (e.g., fixed IP)
Enter the IP address, subnet mask, and gateway
Apply the changes and restart (power cycle) the drive