המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Video: Installing BACnet Driver for PowerSCADA Expert
Issue
Adding a BACnet device to the SCADA project requires the BACnet driver to be installed.

Product Line
EcoStruxure™ Power SCADA Operation 8.2
PowerSCADA Expert

Environment
Windows Installer

Cause
Installing BACnet driver and Cimetrics BACstac protocol stack to support the device that communicates through BACnet driver.

Resolution
Adding a BACnet device to the SCADA project requires the BACnet driver to be installed. The following video with depict the process of installing the driver.

Video description:
1. BACnet driver installation
2. BACstac protocol stack installation
3. Removal of virtual port and selection of physical port
4. Correct port selection verification
5. How to modify BACstac using the batch file once installation is finished

NOTE: It is the responsibility of the installer to verify correct version of the BACnet driver is being installed for any specific version of PSE. All versions go through the same installation process.