איך נוכל לעזור לך היום?

What is the maximum capacity of BMENOC0301 sending MBTCP packets?

Question:
What is the maximum capacity of BMENOC0301 sending MBTCP packets?
Answer:
BMENOC0301 can handle 12000 packets in maximum per second.