איך נוכל לעזור לך היום?

What is the addressing format for using function block Print_Char with NOM communication on M580 X80 rack?

Question:
What is the addressing format for using function block Print_Char with NOM communication on X80 rack?
Answer:
the address of Print_Char should be written via ADDMX block, and the addressing format is like: '0.0.3{192.168.11.3}\\0.2.0.SYS'
192.168.11.3 is the IPaddress of X80 CRA.