איך נוכל לעזור לך היום?

Can BMXCPS4002(AC) and BMXCPS4022(DC) be used together on one redundant backplane?

Question:
Can BMXCPS4002(AC) and BMXCPS4022(DC) be used together on one redundant backplane?
Answer:
Yes, it is allowed.