המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can we have different DNP sever sessions to talk with different SCADA clients
Question:
Can we have different DNP sever sessions to talk with different SCADA clients. Cause customer has two SCADA clients & they have respective master/slave address.


Answer:
No.
DNP3 as TCP server only supports one session with one set of master/slave address.
So customer has to adjust the two clients as same master/slave address to talk with the common session in NOR.
If they would like two customized sessions at NOR part, two NOR modules are needed.