המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can you use the Energy Savings (nLd) motor control type on the ATV930 drive run a constant torque load like a grain leg?

Issue:
Apply nLd energy savings motor control type on a ATV930 to run at constant torque load.

Product Line:
ATV930 in nld motor control type nld

Environment:
All

Cause:
NA

Resolution:
No, nLd control law is not recommended for constant torque or heavy duty applications.


Photo2

Constant torque or Heavy Duty applications will rarely operate in  a condition where the drive is able to reduce the motor current, and using this mode may result in poor speed/torque regulation in those applications.
This mode is primarily intended for fan or pump loads.