המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What are possible causes for DB Unit Short Circuit Fault on ATV930 drive?

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

Issue:
Possible causes for DB Unit Short Circuit Fault on ATV930 drive

Product Line:
ATV930, Altivar 930

Environment:
All

Cause:
NA

Resolution:
The fault may occur if the DB Transistor is shorted. Perform a diode check across PA to PB to check if Transistor is shorted. Also, check BrA is set to Yes.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:Support | Schneider Electric Global (se.com)