המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What are the supported SD cards for a M221 controller?

The supported types of SD cards are: Standard Capacity SD (SDSC), 2GB max or High Capacity SDHC, 32 GB max. Use only SD cards formatted using FAT or FAT32

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)