המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Video: How can I verify logs are catching up or being recorded?
Issue
Verification needed to see if data logs are catching up or recording.

Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
EcoStruxure™ Power Monitoring Expert

Cause
There can be multiple causes that can cause a Data Recorder State to be reset including but not limited to Firmware Upgrades, Driver updates, and Data Alignment.