המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
PME - unable to install with SQL Server Evaluation Edition

Issue
Error checking SQL Server Edition when trying to install PME.

Product Line
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment
Installation

Cause
The PME installer is not configured to recognize SQL Server Evaluation Edition as a valid SQL Server installation.

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

*Note: The Evaluation Editions are not supported indefinitely, and a full license will be required for SQL and the software to continue working.


1. Check the installed SQL Evaluation Edition version by logging into SQL Server Management Studio and running the query: select @@VERSION
2. Copy the .iso file contents to a folder on the local hard drive, then copy the ‘Database.Core.broker.xml’ from the 'Setup/BrokerFragments' folder to a separate folder as a backup.
3. Open ‘Database.Core.broker.xml’ (located in ‘Setup/BrokerFragments’) using Notepad and go to section ‘RequiredSQLEdition’.

default Database.Core.Broker.xml file

4. In the above section, update the required SQL Evaluation Edition as noted in step 1. Below is the example for SQL Enterprise Evaluation (64-bit).

Edited Database.Core.Broker.xml file
5. Save the Database.Core.broker.xml file.

6. Run the MainSetup.exe in the folder with the .iso files copied during step 2, to continue the installation.

Attached is the example broker file configured for PME 8.2 with SQL Server 2016 Evaluation Edition.

שניידר אלקטריק ישראל

קבצים מצורפים
Database.Core.broker.xml.zip [10.93 KB]