המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What are the part numbers for the LED pilot light bulbs used in an ATV61 E-Flex?
Issue:
Part numbers for the LED pilot light bulbs used in an ATV61 E-Flex.

Product Line:
Altivar 61 E-Flex enclosed drives

Environment:
460V, 208V, 230V models

Cause:
Replacement of LED bulbs

Resolution:
Pilot Light Red LED 25501-00003
Head ZB5AV04

Pilot Light Yellow LED 25501-00004
Head ZB5AV05

Pilot Light Green LED 25501-00005
Head ZB5AV03

Note: Long life 120 V LED type bulbs (100,000 hours) are provided as standard hardware from the factory. An alternative to the LEDs are incandescent bulbs (2,000 hours). Part number DL1CE130, Type BA9 rated 120–130 V, 2.4 W, is available as an interchangeable part.


This information can be found in the Renewable Parts section of the E-Flex Instruction Bulletin, which is attached to this FAQ.

שניידר אלקטריק ישראל

קבצים מצורפים
E-Flex Instruction Manual 30072-451-51.pdf [5.87 MB]