המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Intermittent Communications to EM4800 in Power Monitoring Expert 8.1
Issue
The EM4800 communications are intermittent despite being able to continuously ping the device

Product Line
EM4800

Environment
Power Monitoring Expert 8.1

Cause
The communications are slower on the network that the device is on than anticipated

Resolution
Go to devices in Management console.
Right click on the device and click properties.
Right click in the white space and select advanced properties.
Change the Receive Timeout from 10,000 to 20,000.