המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Video: Creating Write_Var Function for FC15 Write Multiple Coils in Unity

This procedure is prepared with Unity Pro v12 software and covers creating a FBD logic section for the M340 Write_Var function block performing a FC15 Write Multiple Coils operation from the BMXNOE0100 ethernet module to an ethernet server device which supports a Modbus FC15 operation.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)