המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Does BMENOC0301 support hold the last value
Question:
Customer has setup his M580 NOC0301 comm with another PLC's NOC using Ethernet IP.
Comm is working all good, however, on his Local Slave side, he wants to be able to change Input Fallback Mode from Set to Zero to Hold the last value but it appears it is grayed out.
Does BMENOC0301 support hold the last value?


Answer:
No, In its current implementation, Ethernet/IP scanner does not support "hold the last value" as input fallback strategy for EIP Devices.